Error-Proofing TIM Application for EV Battery Packs - Chomerics Division | Parker US
How to Ground Electronics

EV OEMs needed a high-performing thermal pad to manage high temperatures within battery packs while adhering to a fully automated manufacturing process.

Summary

To ensure electric vehicle (EV) batteries operate safely and efficiently, temperatures within the battery electronic control unit must be carefully and proactively managed. THERM-A-GAP PAD 30 Thermally Conductive Gap Filler Pads from Parker Chomerics provide a high-performing solution that fits seamlessly into robotic assembly processes, leading to a faster, more efficient assembly line that remains debris-free. 

Parker Image

Customer Challenges/Requirements

Effective thermal management is a top concern for EV original equipment manufacturers (OEMs). Choosing the right thermal interface material (TIM) for the battery electronic control unit is a must, as the battery packs within EVs generate a lot of heat and their performance is directly tied to internal temperatures.

Cleanliness within the manufacturing process is another important factor. Robotics are utilized to prevent the operator from physically touching any of the parts and potentially introducing foreign object debris (FOD), so any thermal pad utilized must fit seamlessly into this assembly. 

Design Requirements

In addition to performance and robotic-compatibility, packaging was a key part of the design. The orientation of thermal pads means extreme care must be taken to ensure they are packaged and shipped safely.

Parker Image

Solution

Parker Chomerics THERM-A-GAP PAD 30 Thermally Conductive Gap Filler Pads checked all the boxes for this application, providing exceptional conformability at a competitive cost. Parker Chomerics also designed a special packaging to make sure everything went smoothly with product shipment.

THERM-A-GAP PAD 30 provides a soft (34 Shore 00) solution with 3.2 W/m-K of thermal conductivity. Additionally, it offers extremely low outgassing, ensuring effective thermal interface between heat sinks and electronic devices where there are uneven surfaces, air gaps and rough surface textures.

THERM-A-GAP pads are easily seen by vision sensors for effective quality control and speed of assembly. They also release effortlessly from the liner for pick-and-place robots, making them ideal for high-volume applications.

Results

With THERM-A-GAP PAD 30, we converted a high-performing TIM pad into a format that is easier to install, increasing assembly-line accuracy. Now applicators are able to properly put pads into the locating fixture without having to touch them, ensuring no foreign debris is introduced while improving the manufacturing time and reducing failure rate.

To ensure zero defects, automated inspection systems check the dimensionality of the pads as well as their location, halting the assembly process if either check reveals a problem.

With THERM-A-GAP PAD 30, OEMs have a solution that combines high performance with ease of assembly and zero defects. 

Parker Image

Let's Get Started

Parker Chomerics offers the products, technical know-how, customer support and supply chain capabilities to meet your challenges and deliver superior, reliable and cost-effective solutions.

THERM-A-GAP PAD 30

Parker Chomerics THERM-A-GAP PAD 30 Thermally Conductive Gap Filler Pads provide a soft (34 Shore 00) solution with 3.2 W/m-K of thermal conductivity.

How to Choose the Right Plastic

On-Demand Webinar: Electric Vehicle Battery Enclosures: Press-in-Place and Custom Sealing Solutions

Electric vehicle battery covers pose unique sealing challenges in the automotive industry. The significant size of the sealing perimeter, the materials and size of the seal mating hardware, and the aggressive performance requirements all play a crucial role in the design and installation of this critical seal. Join our experts to discuss the benefits and innovative sealing options Parker offers to ensure maximum seal life and performance in addition to installation efficiency and cost reduction. 

Parker Image

Automotive Innovative Solutions That Matter

Our global customers rely on us to provide innovative ideas and material solutions. We work with OEMs and Tier automotive suppliers to solve complex electronics and design challenges.

We have an extensive range of products that are used for advanced driver assistance systems (ADAS), electrification cooling systems, metal to plastic light weighting and electrical grounding. Our automotive team has been involved in the design and development of many products including electronics packaging, chassis & body systems, suspension components and engine components. We also offer a range of solutions for internal combustion engines, electric motors, generators and battery packs.

red car driving on paved road

Our products are used in a wide range of industries.


 

Thermal Interface Materials & EMI Shielding Solutions

With more than 60 years of experience, we have the technical know-how to meet the rapidly increasing needs of engineers.

Can't find what you're looking for? Talk to one of our experts.